Troubleshoot the GoldVIP setup on the S32G-VNP-RDB3 demo board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Troubleshoot the GoldVIP setup on the S32G-VNP-RDB3 demo board

Jump to solution
4,500 Views
DRAVE
Contributor IV

Hi NXP,

We are setting up the GOLDVIP development environment. We set up the GoldVIP Yocto project in accordance with Section 25 of document GoldVIP-S32G3-1.12.0-user-manual.pdf. We could not find the HSE firmware release. Can you tell me what to do?

1. We installed HSE-FW_S32G3XX_0_2_22_0.exe in windows and packaged the installation directory under ubuntu20.04 linux.

2. Configure local.conf:

DRAVE_0-1733727197982.png

3. bitbake fsl-image-goldvip

The following error occurs:

DRAVE_1-1733727270507.png

 

Can you tell me what the problem is? Thank you!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
4,393 Views
GuilhermeS32G
Contributor IV

Hello @DRAVE ,

 

For being able to successfully downloading the Docker image without using VPN, please update the Yocto recipe

meta-gvip/recipes-containers/k3s/k3s_%.bbappend

 

By replacing lines 44 and 45 by:

skopeo --override-arch arm64 copy --additional-tag="docker.io/${PAUSE_CONTAINER_TAG}" \
        docker://dockerpull.org/${PAUSE_CONTAINER_TAG} docker-archive:${WORKDIR}/pause-container.tar

This should tell skopeo to use a Docker Registry mirror (dockerpull.org) instead of the default option. This should do the trick.

 

Best regards,

Guilherme

View solution in original post

0 Kudos
Reply
7 Replies
4,473 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @DRAVE 

Thanks for your post.

I suggest modify the local.conf with the following line:

NXP_FIRMWARE_LOCAL_DIR = "/home/workspace/S32G"

You may edit it and retry the Yocto building.

 

BR

Chenyin

0 Kudos
Reply
4,452 Views
DRAVE
Contributor IV

Hi @chenyin_h 

No errors are reported after I configure NXP_FIRMWARE_LOCAL_DIR according to your suggestions. I have a new problem. I can't seem to get xml-commons-resolver1.1-native-1.2-r1, xalan-j-native-2.7.1-r2, and avalon-framework-api-native-4.3-r1.

DRAVE_0-1733795466146.png

The website is as follows:

https://archive.apache.org/dist/xml/commons/xml-commons-resolver-1.2.tar.gz

https://archive.apache.org/dist/xml/xalan-j/xalan-j_2_7_1-src.tar.gz

https://archive.apache.org/dist/excalibur/avalon-framework/source/avalon-framework-api-4.3-src.tar.g...

 

I also couldn't get the file using Google Chrome under windows:

DRAVE_1-1733795668218.png

Do not have permission to access this resource?

Can you help me find out why? Thank you!

Tags (2)
0 Kudos
Reply
4,435 Views
GuilhermeS32G
Contributor IV

Hello @DRAVE ,

 

These missing files can be downloaded through the Web Archive or through mirrors.

  • xml-commons-resolver: link
  • xalan: link 
  • avalon-framework-api: link

 

 

As you may need a VPN for downloading these files, I attached them to the reply.

Once downloaded, place them in your Downloads folder.

 

Best regards,

Guilherme

0 Kudos
Reply
4,421 Views
DRAVE
Contributor IV

Hi @GuilhermeS32G 

Thank you for your reply! I put them in my downloads folder and that problem is solved. I have a new problem. Problems with compiling k3s:

DRAVE_0-1733816525924.png

log:

Initialising tasks: 100% |############################################################################################################| Time
Sstate summary: Wanted 21 Local 0 Mirrors 0 Missed 21 Current 3593 (0% match, 99% complete)
NOTE: Executing Tasks
ERROR: k3s-v1.25.8+k3s1-r0 do_fetch_pause_container: ExecutionError('/home/workspace/s32g/nxp-yocto-goldvip/build_s32g399ardb3goldvip/tmp/woa53-crypto-fsl-linux/k3s/v1.25.8+k3s1-r0/temp/run.do_fetch_pause_container.32385', 1, None, None)
ERROR: Logfile of failure stored in: /home/workspace/s32g/nxp-yocto-goldvip/build_s32g399ardb3goldvip/tmp/work/cortexa53-crypto-fsl-linux/k3+k3s1-r0/temp/log.do_fetch_pause_container.32385
Log data follows:
| DEBUG: Executing shell function do_fetch_pause_container
| time="2024-12-10T07:39:11Z" level=fatal msg="initializing source docker://rancher/mirrored-pause:3.6: pinging container registry registry-io: Get \"https://registry-1.docker.io/v2/\": dial tcp: lookup registry-1.docker.io on 10.86.240.241:53: read udp 172.17.0.8:40057->10.86.24 i/o timeout"
| WARNING: /home/workspace/s32g/nxp-yocto-goldvip/build_s32g399ardb3goldvip/tmp/work/cortexa53-crypto-fsl-linux/k3s/v1.25.8+k3s1-r0/temp/run_pause_container.32385:164 exit 1 from 'skopeo --override-arch arm64 copy --additional-tag="docker.io/rancher/mirrored-pause:3.6" docker://rrrored-pause:3.6 docker-archive:/home/workspace/s32g/nxp-yocto-goldvip/build_s32g399ardb3goldvip/tmp/work/cortexa53-crypto-fsl-linux/k3s/v1.-r0/pause-container.tar'
| WARNING: Backtrace (BB generated script):
| #1: do_fetch_pause_container, /home/workspace/s32g/nxp-yocto-goldvip/build_s32g399ardb3goldvip/tmp/work/cortexa53-crypto-fsl-linux/k8+k3s1-r0/temp/run.do_fetch_pause_container.32385, line 164
| #2: main, /home/workspace/s32g/nxp-yocto-goldvip/build_s32g399ardb3goldvip/tmp/work/cortexa53-crypto-fsl-linux/k3s/v1.25.8+k3s1-r0/to_fetch_pause_container.32385, line 168
ERROR: Task (/home/workspace/s32g/nxp-yocto-goldvip/sources/meta-virtualization/recipes-containers/k3s/k3s_git.bb:do_fetch_pause_container) th exit code '1'
NOTE: Tasks Summary: Attempted 8504 tasks of which 8498 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/workspace/s32g/nxp-yocto-goldvip/sources/meta-virtualization/recipes-containers/k3s/k3s_git.bb:do_fetch_pause_container
Summary: There was 1 ERROR message, returning a non-zero exit code.
Bitbake failed

Do I need a VPN to download these K3s files? Could you please send me the relevant documents of k3s? Thank you!

 

Tags (1)
0 Kudos
Reply
4,417 Views
GuilhermeS32G
Contributor IV

Hello @DRAVE ,

 

The error that you are seeing refer to the following Yocto recipe:

https://github.com/nxp-auto-goldvip/meta-gvip/blob/develop/recipes-containers/k3s/k3s_%25.bbappend#L...

 

More specifically, to this part:

do_fetch_pause_container() {
    rm -f ${WORKDIR}/pause-container.tar
    skopeo --override-arch arm64 copy --additional-tag="docker.io/${PAUSE_CONTAINER_TAG}" \
        docker://${PAUSE_CONTAINER_TAG} docker-archive:${WORKDIR}/pause-container.tar
}

It is attempting to use the Skopeo tool for copying the Docker image rancher/mirrored-pause:3.6. However, the address https://registry-1.docker.io/v2/ is blocked in China.

If you have the option of using a VPN to fetch this file, this would be the easiest approach.

I will take a look and see if there is a way to manually bypass this step. If I find something, I will give you a feedback.

 

Best regards,

Guilherme

0 Kudos
Reply
4,394 Views
GuilhermeS32G
Contributor IV

Hello @DRAVE ,

 

For being able to successfully downloading the Docker image without using VPN, please update the Yocto recipe

meta-gvip/recipes-containers/k3s/k3s_%.bbappend

 

By replacing lines 44 and 45 by:

skopeo --override-arch arm64 copy --additional-tag="docker.io/${PAUSE_CONTAINER_TAG}" \
        docker://dockerpull.org/${PAUSE_CONTAINER_TAG} docker-archive:${WORKDIR}/pause-container.tar

This should tell skopeo to use a Docker Registry mirror (dockerpull.org) instead of the default option. This should do the trick.

 

Best regards,

Guilherme

0 Kudos
Reply
4,379 Views
DRAVE
Contributor IV

Hi @GuilhermeS32G 

Thank you for your reply. I do as your method. I successfully built the GoldVIP Yocto project. Thank you very much! 

DRAVE_0-1733886203611.png

 

 

0 Kudos
Reply