S32G399 Micron NOR Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G399 Micron NOR Flash

1,866 Views
JalseyXie
Contributor II

Hi NXP team,

Our custom board has Micron MT35XU512ABA1G12-0AUT Nor Flash for S32G399. 

But the algorithm of this flash is not listed in the S32 Flash Tool, so we can't flash the binary to external flash.

What's the required steps we need to be able to use the micron NOR flash?

Thanks. 

Tags (1)
0 Kudos
Reply
5 Replies

1,697 Views
db16122
Contributor IV

The difference between MT35XU512ABA1G12 and MT35XU02GCBA could be the die structure internal.

For 512Mb and 2G, the difference would be A/1 die per chip and C/4 die per chip.

So the address range for each device could be different and it may need to be modified

0 Kudos
Reply

1,630 Views
JalseyXie
Contributor II

Hi @db16122 ,

Thanks for explaining.

We managed to make a new algorithm and added to the S32 flash tool/

Regards.

0 Kudos
Reply

1,841 Views
Joey_z
NXP Employee
NXP Employee

hi,JalseyXie

Thank you for contacting us.

Generally, different models of Flash from the same manufacturer will use the same command words and the same register design.

You can try to use the MT35XU02GCBA.bin file.

Joey_z_0-1748312033128.png

In addition, you can refer to the document for the new Flash tool algorithm image.

S32G_ADD_GDFLASH_SUPPORT - NXP Community

This document is a community document and can be used as a reference.

Hope it can help you.

BR

Joey

0 Kudos
Reply

1,821 Views
JalseyXie
Contributor II

Hi @Joey_z ,

Thanks for the reply. I did try the algorithm you mentioned, but it's not compatible with the Micron NOR flash. 

I'll will check the document to make new algorithm.

Regards,

0 Kudos
Reply

1,810 Views
Joey_z
NXP Employee
NXP Employee

hi,JalseyXie

Ok,I am glad to support you.

BR

Joey

0 Kudos
Reply