S32G3 network interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G3 network interface

跳至解决方案
627 次查看
JasonTseng
Contributor I

S32G3 block diagram shows 

Networking: 

4x FlexCAN
3x LINFlexD

1x 2-channel FlexRay

1x GMAC                   <--- this one
1x USBOTG
2x SerDes with PCIe 3.0 and 2 lanes each

 

Ethernet networks:

PFE, IEEE 1588v2 + AVB and three 2.5 Gbit MAC 

 

So my question is what is the difference and/or relationship between 

GMAC and 2.5Gbit Mac?

 

Thanks

 

 

0 项奖励
回复
1 解答
600 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @JasonTseng

Thanks for the questions.

There are two kinds of ethernet interface on S32G3, one is called GMAC, the other one is called PFE, the 2.5G there means that the PFE could support on three ports at 2.5G network.

 

Best Regards

Chenyin

在原帖中查看解决方案

0 项奖励
回复
4 回复数
592 次查看
chenyin_h
NXP Employee
NXP Employee

Thanks for using NXP products, it is my pleasure to help.

 

Best Regards

Chenyin

0 项奖励
回复
593 次查看
JasonTseng
Contributor I

OK, understood, thank you.

0 项奖励
回复
601 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @JasonTseng

Thanks for the questions.

There are two kinds of ethernet interface on S32G3, one is called GMAC, the other one is called PFE, the 2.5G there means that the PFE could support on three ports at 2.5G network.

 

Best Regards

Chenyin

0 项奖励
回复
604 次查看
JasonTseng
Contributor I

ps: I am referring PBS32G3V2.pdf p. 2 block diagram 

0 项奖励
回复