S32G3 NXP BOOTLOADER WITH SECURE BOOT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G3 NXP BOOTLOADER WITH SECURE BOOT

1,063件の閲覧回数
kavyapk
Contributor I

Hello Team,

I am using Board: S32G399RDB3 with an AUTOSAR application and NXP Boot on the M7 core.

HSE vesrion:HSE_DEMOAPP_S32G3XX_0_2_51_0

I am configuring secure boot for NXP bootloader and configuring both primary and back application bootloader.So when I am coruupting primary bootloader and checking whwether it is loading from backup,I am able to load from backup and application is running.

but during this time I am checking the api HSE_GetCoreStatus,I am observing the below status.

corestatus.PNG

Could you please help to decode this status.

0 件の賞賛
返信
1 返信

1,041件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @kavyapk 

Thanks for the post.

From the code shown, the following part from service API reference manual could be useful for your reference.

chenyin_h_0-1743566228954.png

 

BR

Chenyin

 

0 件の賞賛
返信