S32G3 Internal RTC as WKUP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G3 Internal RTC as WKUP

跳至解决方案
1,986 次查看
wjb
Contributor I

Do you have a similar example as: "S32K344_Standby_RTC_Wakeup_Example"  for s32g3, using the internal RTC as wakeup source?

I am using board S32G-VNP-RDB3.

Thank you. -w

0 项奖励
回复
1 解答
1,954 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The available example for RTC as wakeup source is provided under Linux itself, which is run under the A53 core.

Are you looking for an M7 example?

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,955 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The available example for RTC as wakeup source is provided under Linux itself, which is run under the A53 core.

Are you looking for an M7 example?

Please, let us know.

0 项奖励
回复