S32G3 GoldVIP Engineering Bulletin (EB00942)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G3 GoldVIP Engineering Bulletin (EB00942)

Jump to solution
4,094 Views
Jasmin_IM
Contributor III

Hi,

I read the EB00942 and wanted to follow the instructions and configure the NoC QoS as stated in the document, only to find, that the GoldVIP version mentioned is not available for download?

Jasmin_IM_0-1732031443060.png

The EB00942 states, that GoldVIP 1.13.0 onwards should be used, I am only able to see GoldVIP 1.12.0 in the download section. Where is the 1.13.0 located?

Jasmin_IM_1-1732031470574.png

Thank you

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,828 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @Jasmin_IM,

The GoldVIP 1.13 is already published. So now, you can follow the EB00942 without problems. 

View solution in original post

7 Replies
4,057 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @Jasmin_IM, the GoldVIP 1.13.0 will be publish in the next couple of weeks. 

 

4,048 Views
Jasmin_IM
Contributor III
sounds good, thank you.
0 Kudos
Reply
4,041 Views
carlos_o
NXP TechSupport
NXP TechSupport

Let me know if there is anything else I can do for you

0 Kudos
Reply
4,004 Views
Jasmin_IM
Contributor III
as of now, that would be all. As soon as the 1.13.0 version is available we can close the ticket. Thank you for your help and wish you a nice start to the week.
0 Kudos
Reply
3,829 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @Jasmin_IM,

The GoldVIP 1.13 is already published. So now, you can follow the EB00942 without problems. 

3,755 Views
Jasmin_IM
Contributor III
thank you
0 Kudos
Reply
4,078 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @Jasmin_IM,

I will review with the internal team why this version is not published. 

This can take some time; I appreciate your patience.

I will come back with more information ASAP.