[S32G274 RDB2] [IPCF 4.6] M7 start success,linux kernel panic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32G274 RDB2] [IPCF 4.6] M7 start success,linux kernel panic

2,084件の閲覧回数
NicholasZheng
Contributor II

Hello,

    I download BSP35.0,and reference SW32G_IPCF_4.6.0_D2205_UserManual.pdf,add the IPCF feature in  Image,  and the image has been built successful.

    This image has been burned to SD card,and image can be start normally.(Not hit anykey after power on the RDB2 board)

    But when I boot M7(bin file is IPCF_Example_S32G274A_M7_0.bin),and then boot linux,the kernel panic,how can i slove this problom.

IPCF UserManual:

NicholasZheng_0-1683249300484.png

Error Serial log:

=> startm7 0x34501000
Starting CM7_0 core at SRAM address 0x34501000 ... done.
=> boot
PFEng firmware file 'mmc@0:1:s32g_pfe_class.fw' loading failed: -2
PFE: emac0: sgmii emac1: none emac2: rgmii
pfeng_cfg_mode_enable: Invalid PFE device
switch to partitions #0, OK
mmc0 is current device
13758472 bytes read in 624 ms (21 MiB/s)
Booting from mmc ...
44501 bytes read in 21 ms (2 MiB/s)
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 0000000083000000, end 000000008300ddd4
fixup: pfe0 set to 00:01:be:be:ef:11
fixup: pfe1 set to 00:01:be:be:ef:22
fixup: pfe2 set to 00:01:be:be:ef:33

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.145-rt74+g1594b25154a2 (oe-user@oe-host) (aarch64-fsl-linux-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.35.1) #1 SMP PREEMPT Tue Nov 29 10:33:39 UTC 2022
[ 0.000000] Machine model: NXP S32G274A-RDB2
[ 0.000000] earlycon: linflex0 at MMIO 0x00000000401c8000 (options '115200n8')
[ 0.000000] printk: bootconsole [linflex0] enabled
[ 0.000000] SError Interrupt on CPU0, code 0xbf000000 -- SError
[ 0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 5.10.145-rt74+g1594b25154a2 #1
[ 0.000000] Hardware name: NXP S32G274A-RDB2 (DT)
[ 0.000000] pstate: 60000085 (nZCv daIf -PAN -UAO -TCO BTYPE=--)
[ 0.000000] pc : setup_arch+0x164/0x58c
[ 0.000000] lr : setup_arch+0x15c/0x58c
[ 0.000000] sp : ffffffc010c83ef0
[ 0.000000] x29: ffffffc010c83ef0 x28: 0000000080b40018
[ 0.000000] x27: 00000000ffaa27f8 x26: 0000000000000000
[ 0.000000] x25: 00000000ffb39a20 x24: 00000000ffe03f18
[ 0.000000] x23: ffffffc010d23000 x22: ffffffc010c8e380
[ 0.000000] x21: fffffffefe600094 x20: ffffffc010cd7158
[ 0.000000] x19: ffffffc010000000 x18: 0000000000000030
[ 0.000000] x17: 0000000000001800 x16: 0000000000000000
[ 0.000000] x15: ffffffc010c8e7e8 x14: ffffffffffffffff
[ 0.000000] x13: 0000000000000000 x12: 0000000000000028
[ 0.000000] x11: 0000000000000015 x10: 0101010101010101
[ 0.000000] x9 : 3334ff6b6e6e6f5e x8 : 7f7f7f7f7f7f7f7f
[ 0.000000] x7 : 736d647164676e62 x6 : 000006161d090b74
[ 0.000000] x5 : 740b091d16060000 x4 : 0000000000000000
[ 0.000000] x3 : ce6ded8ca0000000 x2 : 000000000000000c
[ 0.000000] x1 : 0000000000000000 x0 : 0000000000000080
[ 0.000000] Kernel panic - not syncing:
[ 0.000000] Asynchronous SError Interrupt
[ 0.000000] ---[ end Kernel panic - not syncing: Asynchronous SError Interrupt ]---

 

 

タグ(2)
0 件の賞賛
返信
1 返信

1,923件の閲覧回数
tianwei
Contributor I
Hello, has this been resolved? I also encountered the same problem
0 件の賞賛
返信