S32G2 doesn't work and RST ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2 doesn't work and RST ERROR

3,730 Views
zhipeng
Contributor III

I use S32G2 and its PMIC (VR5510) ,Refer to the S32G-VNP-RDB2 scheme.

The voltages are correct.

zhipeng_0-1756981912428.png

But the S32G2 does not work

zhipeng_3-1756982184533.png

 

zhipeng_2-1756982115368.png

The system image is in the TF card, and LPDDR is not installed yet

What could be the problem? 

##S32G-VNP-RDB  S32G2 

 

 

 

 

0 Kudos
Reply
7 Replies

3,595 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @zhipeng 

Thanks for your reply.

1. You are willing to booting the board via SD, is it right? if yes, also measure the clock of SD

2. From the wave you captured, seems there is abnormal pull-down signal on RESET_B.

3. If confirmed no issues from HW, use the debugger to attach to the board for further analysis.

 

BR

Chenyin

0 Kudos
Reply

3,560 Views
zhipeng
Contributor III

Hi Chenyin,

    Thanks for the reply. 

    Yes,I am willing to booting the board via SD,The captured waveform is as follows.

zhipeng_1-1757412345430.png

2. There is no pull-down HW setting on RESET_B.

 

3. Can I use S32 Debug Probe debugger?

zhipeng_0-1757408456653.png

    Thanks very much!

    BR.

 

0 Kudos
Reply

3,519 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @zhipeng 

Thanks for the reply.

Yes, the S32Debug probe could be used for the S32G2 via JTAG interface

 

BR

Chenyin

0 Kudos
Reply

3,104 Views
zhipeng
Contributor III

Hello,  chenyin_h

Thanks for the reply.

I have bought the debugger. Using it, can run MCU programs on the M7 core, but the A5 core still cannot run the system. Do I need any additional configuration or programming?

BR

0 Kudos
Reply

3,696 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @zhipeng 

Thanks for your post.

So the schematic of your custom board is similar to RDB2, but without LPDDR4 installed? The DDR interface pins are left unconnected on board?

What kind of the image on the TF card? how they are generated?

 

BR

Chenyin

0 Kudos
Reply

3,687 Views
zhipeng
Contributor III

Hi Chenyin,

Thanks for the reply.

The schematic of my custom board is similar to RDB2,but because of the DDR hasn't been bought yet, it is not installed。The DDR interface pins are left unconnected on board。

the image on the TF card  is made by the installation instructions, the following two, are the same problem.

1. 

zhipeng_0-1757057993977.png

2.

zhipeng_1-1757058013701.png

What could be the problem? 

Thanks very much!

 

BR

 

0 Kudos
Reply

3,606 Views
zhipeng
Contributor III
The specific model is S32G274AABK0VUCT.
0 Kudos
Reply