S32G2-VNP-RDB2 for Core M7, Application gateway

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2-VNP-RDB2 for Core M7, Application gateway

Jump to solution
2,571 Views
Balavanth_1993
Contributor I

Hi Community,

I am working on S32G274A RDB2 board for M7 core,  for our gateway project, i needed firmwares like LLCE,PFE and HSE, and i have installed Automotive
Software Package Manager, but still i am not getting particular documents for core M7 and gateway, could anyone suggest how to get a flow on M7.

Thanks in advance,

Balavanth.

 

0 Kudos
Reply
1 Solution
2,539 Views
bpe
NXP Employee
NXP Employee

Automotive Software Package Manger is an online tool. You cannot download it.
After you select packages to download, it offers you two files, one is a self-
extractor to install, another is a Manual. Make sure you saved both of them.
Follow the Manual to install the package(s) you selected. More information is
available in each package's installation directory. For ARM M7 core details,
Arm Cortex-M7 Processor Technical Reference Manual, DDI 0489D Revision r1p1. 

Best Regards,
Platon

 

 

View solution in original post

0 Kudos
Reply
1 Reply
2,540 Views
bpe
NXP Employee
NXP Employee

Automotive Software Package Manger is an online tool. You cannot download it.
After you select packages to download, it offers you two files, one is a self-
extractor to install, another is a Manual. Make sure you saved both of them.
Follow the Manual to install the package(s) you selected. More information is
available in each package's installation directory. For ARM M7 core details,
Arm Cortex-M7 Processor Technical Reference Manual, DDI 0489D Revision r1p1. 

Best Regards,
Platon

 

 

0 Kudos
Reply