S32G2 UART(ttyLF1) Not Working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2 UART(ttyLF1) Not Working

1,674件の閲覧回数
vimalrajendran
Contributor II

Hi,

          i am using S32G2 board. i tried to enable ttyLF1(uart). but it is not working. can you give me some suggections.

 

 

Thanks

Vimal

タグ(1)
0 件の賞賛
返信
1 返信

1,651件の閲覧回数
bpe
NXP Employee
NXP Employee

No suggestions can be given based on the information you provided, sorry.
If you wish NXP Technical Support to help you, please provide a reasonably
detailed problem description. The following is the minimum recommended details:

  1. The exact model of NXP development board you are working with,
    if applicable.
  2. If the problem is observed in Linux environment, the version of NXP Automotive
    Linux BSP.
  3. A compact description of your actions, the expected result, the observed
    result, why you think what you observed was not correct.
  4. If the system outputs any error messages, a console log showing the commands
    issued and the system reaction to them.

Best Regards,
Platon

 

0 件の賞賛
返信