S32G2 LLCE message buffers ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2 LLCE message buffers ?

ソリューションへジャンプ
2,001件の閲覧回数
leehaonan
Contributor II

LLCE enablement consist of binary images for the code running on each of the LLCE cores. Support for
16 CAN and 4 LIN communication controllers as it is expected by the AUTOSAR® 4.4 drivers on the
host side.
• Timestamping of received and transmitted frames
• S32G2: Support for up to 1024 filters and 2000 message buffers
• S32G3: Support for up to 4096 filters, 1732 long message buffers and 2364 short message buffers

 

Q:

2000 message buffers

1.Does this 2000 message buffers mean that  it's for each LLCE CAN channel?

 

タグ(1)
0 件の賞賛
返信
1 解決策
1,971件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We do apologize for the delay. Below will be some comments on regards of your questions:

Q1 >> Does this 2000 message buffers mean that it's for each LLCE CAN channel?

A1 >> For the available information, the 2000 message buffers should be for all channels, not for each one. The following is told by the internal team:

"... there are total 2000 Rx MBs which can be flexibly assigned between different channels."

Please, let us know.

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,972件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We do apologize for the delay. Below will be some comments on regards of your questions:

Q1 >> Does this 2000 message buffers mean that it's for each LLCE CAN channel?

A1 >> For the available information, the 2000 message buffers should be for all channels, not for each one. The following is told by the internal team:

"... there are total 2000 Rx MBs which can be flexibly assigned between different channels."

Please, let us know.

 

0 件の賞賛
返信