S32G2 DIAGNOSTICS_BIST failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2 DIAGNOSTICS_BIST failure

2,304 Views
lvaynberg
Contributor I

Hi,

I'm running a BIST_DIAGNOSTIC_CFG on an S32G274A MCU on the RDB2 dev board. I'm observing a BIST_FAILED result, with the following MBIST status flags (corresponding to the MBSSW registers:

MBESW0,1,2,3 registers: FFFFFFFF FFFFFFFF 00003FFF 00000000
MBSSW0,1,2,3 registers: FFFFFFFF FFFFBFFF 00003FFF 00000000

I believe this is indicating that MBIST 46 is failing which corresponds to PCIE_CORE.

In our fleet of S32G274A devices, we've observed that some devices don't fail this test while others do, and some of them fail only sometimes. Is this a known issue with the S32G274A? Is there a particular clock configuration or any other configuration that can cause this MBIST to fail?

 

Thanks in advance.

0 Kudos
Reply
2 Replies

2,193 Views
lvaynberg
Contributor I

Thanks for investigating. It looks like we have an instance on a non ES chip.

 

Chip's marking are as follows:

S32G274ASBVUC

0P77B

SBBB2133B

 

0 Kudos
Reply

2,228 Views
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

we are still trying to investigate it, but we are not able to confirm any issue yet. Please, what silicon version do you use?

0 Kudos
Reply