S32G2 - DDR4 Pin swapping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2 - DDR4 Pin swapping

2,114件の閲覧回数
sangrael
Contributor I

Hi I would like to doublecheck DDR4 pin swapping on S32G2

 

From S32G2HDG: S32G2 Hardware Design Guideline document,

I can see pin swapping allowed between Bytes if there are in the same channel.

But, it doesn't say other what channel the other bites are in

 

sangrael_0-1649805450252.png

The channel is in this order? and for the other byte line there are also in numerical order?

sangrael_1-1649805780670.png

 

 

 

Regards,

Sangrae

 

0 件の賞賛
返信
1 返信

2,025件の閲覧回数
marcuslim
NXP Employee
NXP Employee

Hi Sangrae,

I understood from the Disty engineer that this has been resolved.  If not, please update this ticket.  Thanks.

 

Regards,

Marcus

0 件の賞賛
返信