S32G - debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G - debugger

2,519 Views
chaudhari123
Contributor I

Hi,

I am using S32G. There are Two debugger - Lauterbach and S32 Debug Probe. which is more comfortable and their difference .also any document please share . can u please help me

 thank  and regards,

Snehal123

0 Kudos
Reply
1 Reply

2,504 Views
bpe
NXP Employee
NXP Employee

When S32DS is used with Lauterbach probe, it actually starts Lauterbach debugger
at the project debug stage. The purpose of S32 debugger and Lauterbach debugger
in principle is the same, and basic debug functions are available in the
both, however, their user interfaces are different. It is the question of
your personal preference, which is more convenient to you. If you are interested
in a particular S32G debugger feature, feel free to ask more specifically.
Note that Lauterbach probe and Lauterbach debugger are not NXP products.
We suggest contacting Lautherbach directly for advanced questions about them.

 

Best Regards,
Platon