S32G XPCS error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G XPCS error

Jump to solution
1,949 Views
piaochunri
Contributor II

Hi experts,

I was debugging the s32g399a board.There is error during boot step.The configure is below.And  we do not add GMAC phy actually.

piaochunri_2-1724899981982.jpeg

 

The log is below

piaochunri_1-1724899927990.png

Can you help me to solve this?

 

0 Kudos
Reply
1 Solution
1,894 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @piaochunri 

Thanks for your post

According to serdes working modes in the S32G3RM Rev4, and your specific requirement, seems only mode1 for both serdes0 and serdes1 could fulfill your request.

However, since your were using the BSP39, as indicated below from BSP39 UM

chenyin_h_0-1725246655701.png

 

Mode1 on Serdes0 is not supported.

 

BR

Chenyin

View solution in original post

0 Kudos
Reply
3 Replies
1,895 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @piaochunri 

Thanks for your post

According to serdes working modes in the S32G3RM Rev4, and your specific requirement, seems only mode1 for both serdes0 and serdes1 could fulfill your request.

However, since your were using the BSP39, as indicated below from BSP39 UM

chenyin_h_0-1725246655701.png

 

Mode1 on Serdes0 is not supported.

 

BR

Chenyin

0 Kudos
Reply
1,915 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @piaochunri 

Thanks for you post.

May I know if you are working with the BSP35, would you please share the hwconfig and the pfe_xxx related uboot environments used?

 

BR

Chenyin

0 Kudos
Reply
1,905 Views
piaochunri
Contributor II

Thank you.

We are using bsp 39.0.And the hwconfig is as below.

hwconfig=pcie0:mode=sgmii,clock=ext,fmhz=100,xpcs_mode=0;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=both
 
The result of pri command is as below:

baudrate=115200
boot_mtd=booti
bootargs=root=/dev/ram rw earlycon loglevel=7
bootcmd=s32ccgmac 0 emac sgmii;setenv pfe1_phy_addr 1;s32ccgmac 0 emac sgmii;setenv pfe1_phy_addr 1;mmc dev ${mmcdev}; if mmc rescan; then if run loadii
bootdelay=2
console=ttyLF0
eth1addr=00:04:9f:be:ef:00
eth2addr=00:04:9f:be:ef:01
ethact=ethernet@4033c000
ethaddr=7e:eb:18:eb:d4:2c
fdt_addr=0x83000000
fdt_enable_hs400es=fdt addr ${fdt_addr}; fdt rm /soc/mmc no-1-8-v; fdt resize;
fdt_file=s32g399a-rdb3.dtb
fdt_high=0xffffffffffffffff
fdt_override=;
fdtcontroladdr=ffa96000
flashboot=echo Booting from flash...; run flashbootargs;mtd read Kernel ${loadaddr};mtd read DTB ${fdt_addr};mtd read Rootfs ${ramdisk_addr};${boot_mtd;
flashbootargs=setenv bootargs console=${console},${baudrate} root=/dev/ram rw earlycon ;setenv flashsize 0x04000000;
hwconfig=pcie0:mode=sgmii,clock=ext,fmhz=100,xpcs_mode=0;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=both
image=Image
initrd_high=0xffffffffffffffff
ipaddr=10.0.0.100
loadaddr=0x80000000
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}; run fdt_override;
loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}
loadtftpfdt=tftp ${fdt_addr} ${fdt_file};
loadtftpimage=tftp ${loadaddr} ${image};
mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot} earlycon
mmcboot=echo Booting from mmc ...; run mmcargs; if run loadfdt; then run fdt_fixups; ${boot_mtd} ${loadaddr} - ${fdt_addr}; else echo WARN: Cannot load;
mmcdev=0
mmcpart=1
mmcroot=/dev/mmcblk0p2 rootwait rw
netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp earlycon
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; i;
netmask=255.255.255.0
nfsboot=echo Booting from net using tftp and nfs...; run nfsbootargs;run loadtftpimage; run loadtftpfdt;${boot_mtd} ${loadaddr} - ${fdt_addr};
nfsbootargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs rw ip=${ipaddr}:${serverip}::${netmask}::eth0:off nfsroot=${serverip}:/tftpboon
pfeng_mode=enable,sgmii,rgmii,rgmii
ramdisk_addr=0x90000000
script=boot.scr
serverip=10.0.0.1
stderr=serial@401c8000
stdin=serial@401c8000
stdout=serial@401c8000

Environment size: 2652/8188 bytes

0 Kudos
Reply