S32G-VNP-RDB3: Onchip debugging support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G-VNP-RDB3: Onchip debugging support

488 Views
madhusudangupta007
Contributor I

Hello,

I want to debug my AUTOSAR Operating System based application on following environment.

1) Board Name: S32G-VNP-RDB3

2) Microcontroller Variant: S32G399

3) Cortex-M7 Cores

4) Host: Windows

Is there any on-chip debugging support enabled in the mentioned board where I can connect without any external debugger or probe.

If on-chip debugging support is not available on this board then can I debug with S32 debug probe (H/W) and s32 design studio IDE (S/W) ?

 

With Regards,

Madhusudan Gupta

0 Kudos
Reply
1 Reply

460 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @madhusudangupta007 

Thanks for your post.

1. There is no onchip debugger on RDB3, so it is not supported to directly debug the RDB3 via the USB port.
2. Commonly, the Lauterbach TRACE32 Debug is used for debugging the S32G products, besides, the S32 Debug Probe which is provisioned by NXP(S32 Debug Probe | NXP Semiconductors) is also used.
3. Yes, as mentioned before, the S32 debug probe(HW) and S32 Design Studio(IDE) could be used together for debugging the RDB3 board. 

 

 
BR
Chenyin
0 Kudos
Reply