S32G-VNP-RDB2 LIGHT UP RGB LED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G-VNP-RDB2 LIGHT UP RGB LED

1,597 Views
a_tosetto
Contributor I

Hi,

Hi to all,

 

I'm new on this kind of applications, so I ve to ask help!

I'm following the user guide S32G-VNP-RDB2 SOFTWARE ENABLEMENT GUIDE to create the RBG LED example. I 'm checked all the steps up to page 23. Checked also  (more the once) the switches on the board, but i insert the card, powerup  the board and the RBG led remains blue.

Previously I laoded the linux OS from the SD card provided by NXP and i can see the system boot up normally.

What I'm doing wrong? There is a way to debug the application? I do not have the debug probe, should I ve to buy it?

 

Kind regards,

Andrea  

0 Kudos
Reply
3 Replies

1,570 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @a_tosetto 

Thanks for your post.

For M core related development and debugging on S32G2, we suggest using a debugger for the similar issue faced, currently, the Lauterbach is commonly used for S32G related development, besides, the S32 debug probe could also be used.

 

BR

Chenyin

0 Kudos
Reply

1,557 Views
a_tosetto
Contributor I

Hi,

thank you for the feedback, from a not skilled user like me what is better, Lautebach or S32 Debug probe?

 

Regards,

Andrea

0 Kudos
Reply

1,503 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @a_tosetto 

Thanks for your reply.

1. From NXP's perspective, both debugger could be used on RDB2, there is standalone IDE for Lauterbach, while the S32 debug probe is used with S32DS.

2. From personal experience, for Industry/AUTOSAR development, which is especially working with EB/Vector, etc. The lauterbach is usually used and supported. While only working with S32DS for development, the S32 debug probe could also be used for debugging purpose

 

BR

Chenyin

0 Kudos
Reply