S32G LLCE build 1.0.5QLP1 example pfe failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G LLCE build 1.0.5QLP1 example pfe failed

1,999 Views
hebi
Contributor I

 

Hello,

        I installed the routine of S32G LLCE 1.0.5QLP1 according to the AN13423, LLCE_AF can compile successfully, but LLCE_PFE routine cannot be compiled successfully. I tried comparing the makeflie file of 1.0.4 and found that there is no difference, while 1.0.4 compiles successfully, so is there anything different about debugging the PFE routine of 1.0.5QLP1?

     The following figure shows the error message of compiling the PFE routine of version 1.0.5QLP1

 

 

hebi_0-1695181817515.png

 

Labels (1)
0 Kudos
Reply
3 Replies

1,945 Views
nxf92355
NXP Employee
NXP Employee

Hi 锦荣 何

 

Hope you are doing well

are you seeing such file tmp/Llce_Firmware_load.o  ? and can you tell us which compiler you are using ?

 

Regards ,

Tushar

0 Kudos
Reply

1,864 Views
hebi
Contributor I

Hi  Tushar

     thanks for  your reply .     

     The project cannot generate the tmp folder, I am using the GCC cross-compiler, the specific information is shown in the figure. In addition, the project under the llce_sample_app_af can be compiled successfully.

hebi_0-1696757923309.png

regards,

锦荣,HE

0 Kudos
Reply

1,833 Views
nxf92355
NXP Employee
NXP Employee

Hi 锦荣 何

I was trying to regenerate issue. I am getting tmp folder generated. can you check with the prerequisites as below

- S32_RTD_4.4.4.0.0_D2211

- S32G_LLCE_GATEWAY_4.4_1.0.5_D2212

- PFE RTD 1.0.0

 

Can you try to compile via command line at the location of example C:\NXP\S32G_LLCE_1_0_5_QLP1\sample_app_llce\llce_sample_app_pfe\    and rum make command.

 

Regards ,

Tushar

0 Kudos
Reply