S32G Goldvip CAN usecase hardware setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G Goldvip CAN usecase hardware setup

1,259 Views
Vishnu13
Contributor I

Hi,

I want to test the CAN usecase.

I connected the following pins using wires:

i) FlexCAN0(L) to LLCE-CAN0 (L)

ii) FlexCAN0(H) to LLCE-CAN0 (H)

iii) FlexCAN1(L) to LLCE-CAN1(L)

iv) FlexCAN1(H) to LLCE-CAN1(H)

 

I executed the following script:

./canperf.sh -t can0 -r can1 -i 0 -o 4 -s 64 -g 0 -l 10

 

But the output was not as expected. Attaching the generated report below.

1665062477469(1).jpg

Could you please explain what could be the issue here? Is there any additional hardware requirement? The image used is golvip1.3.0

0 Kudos
Reply
1 Reply

1,253 Views
gmocanu
NXP Employee
NXP Employee

Hello, Vishnu,

 

The fact that the reported M7 core loads are 0% tells me that the application doesn't run at all. Are you sure you booted from QSPI? The SW4.7 DIP switch should be set to OFF.

 

Best regards,

George

0 Kudos
Reply