S32G Freertos 系统是否支持多核

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G Freertos 系统是否支持多核

跳至解决方案
672 次查看
飘飘飘飘
Contributor II

你好,
我们S32G项目中使用Freertos系统开发,基于SW32_FreeRTOS_10_4_6_UOS_4_0_2_DS_updatesite_D2307.zip 和SW32G_S32DS_3.5.1_D2210.zip搭建的S32DS环境,请问下这个版本的Freertos 是否支持多核处理。
比如,Freertos创建一个task让他在指定核上运行。
谢谢

标记 (1)
0 项奖励
回复
1 解答
652 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @飘飘飘飘

Thanks for your question

FreeRTOS version 11.0.0 is the first to merge Symmetric Multiprocessing (SMP) support into the mainline release. I also have checked the document on the latest FreeRTOS release for S32G.

Currently, the SMP is not supported in the project released.

Sorry for any inconvenience.

 

Best Regards

Chenyin

在原帖中查看解决方案

0 项奖励
回复
1 回复
653 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @飘飘飘飘

Thanks for your question

FreeRTOS version 11.0.0 is the first to merge Symmetric Multiprocessing (SMP) support into the mainline release. I also have checked the document on the latest FreeRTOS release for S32G.

Currently, the SMP is not supported in the project released.

Sorry for any inconvenience.

 

Best Regards

Chenyin

0 项奖励
回复