S32DS v3.5 Linux version not found RTD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS v3.5 Linux version not found RTD

1,642 Views
jack_zhangjg
Contributor II

Hi expert,

I'm using S32DS to do DDR training test.
I install S32DS v3.5 linux version on Ubuntu20.04 system following Installation Guide, and it startup&run Okay. 
But I find that there is no RTD package in the "Extentions and Upates" window.
Then I install the same version(v3.5) on Windows 10 system, and I find that there is RTD v4.0.0 package in the "Extentions and Upate" window, and it can be installed.
I compare the "Avalilable S32DS Software Sites" of Preferences menu, but there is no difference.

Does Linux version of S32DS no RTD package? Or I miss something?
I want to install RTD to the S32DS in Ubuntu system to do DDR training test. But I don't know how and where to install it.
Could you help me please ?

Thanks.

0 Kudos
Reply
2 Replies

1,305 Views
adalberto1
Contributor II

I am having the exact problem.

I've installed S32DS 3.5 update 13 in Windows and Linux.  I've installed the development package for the S32K3xx processor, then attempted the installation for the RTD drivers.  In Windows, everything works fine.  In Linux, although the installation completes, I do not see the RTD drivers listed in the "Extensions and Updates" window.  Nor do I see any examples with the RD version I am attempting to load.

What was the resolution to this issue?  Is there an issue using the RTD drivers in S32DS under Linux?  

I am using Ubuntu 20.04, SW32K3_S32DS_3.5.13_D2407.zip, and SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.zip.

I need Linux support because my Windows environment in VirtualBox does not work with the Multilink debugger.

0 Kudos
Reply

1,636 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the following information:

"I compare the "Avalilable S32DS Software Sites" of Preferences menu, but there is no difference."

We understand that there might be a problem where S32DS is not being able to connect to the available sites under Linux. Can you let us know which S32 variant you are working with?

Please, let us know.

0 Kudos
Reply