I refer to the S32G-VNP-RDB2 SOFTWARE ENABLEMENT GUIDE, the suggested software version was SW32G2_S32DS_3.4.0_D2012.zip + S32DS.3.4_b201217_win32.x86_64.exe + Real Time Drivers S32_RTD_4.4_1.0.0_HF01_D2102_DS_Updatesite.zip.
But I actually download S32DS.3.4_b201217_win32.x86_64.exe +SW32G2_S32DS_3.4.1_D2104.zip +SW32G_RTD_4.4_3.0.2_HF01_DS_updatesite_D2204.zip.
When I want to new the Light Up RGB LED and open peripherals tool, It will show "Peripherals: [SDK] Failed to update code - Code generation failed“. I'm not sure if the different software version combination causing these error.