Read FCCU faults S32G3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Read FCCU faults S32G3

Jump to solution
1,598 Views
Harish_R
Contributor III

Hi Team,

Just a quick question. 

How to read FCCU faults. is there any global variable or any register bits updated when the fault is detected.

 

BR

Harish R

0 Kudos
Reply
1 Solution
1,531 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @Harish_R 

It will depend on your configuration, because you can enable the FCCU to triggers an IRQ to solve the fault, if that happen the register clear the NCF fault at the register. You could review the flow of a fault in the Figure 591. Single fault signal flow

 

carlos_o_0-1749760941396.png

[S32G3 Reference Manual, Rev. 4, 02/2024, page 4126]

Also, keep in mind that you need to clear a software-recoverable non-critical faults

carlos_o_1-1749761348772.png

 

 

View solution in original post

0 Kudos
Reply
3 Replies
1,579 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @Harish_R,

The registers you want to read is the 67.7.1.7 Non-critical Fault Status (NCF_S0 - NCF_S3) at the S32G2.

carlos_o_0-1749589076421.png

carlos_o_1-1749589091600.png

[S32G2 Reference Manual, Rev. 8, February 2024, page 3896]

0 Kudos
Reply
1,551 Views
Harish_R
Contributor III

Hi @carlos_o 

Thanks for the info!

so, which means this register should be checked in cyclic to find the reported fault right?

 

Br

Harish R

0 Kudos
Reply
1,532 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @Harish_R 

It will depend on your configuration, because you can enable the FCCU to triggers an IRQ to solve the fault, if that happen the register clear the NCF fault at the register. You could review the flow of a fault in the Figure 591. Single fault signal flow

 

carlos_o_0-1749760941396.png

[S32G3 Reference Manual, Rev. 4, 02/2024, page 4126]

Also, keep in mind that you need to clear a software-recoverable non-critical faults

carlos_o_1-1749761348772.png

 

 

0 Kudos
Reply