Questions about S32G2 CAN gateway

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about S32G2 CAN gateway

1,158件の閲覧回数
pole
Contributor II

We are using S32G2 as the CAN gateway and the LLCE engine is used. What should I do if only specific packets are forwarded?

 

For example, the 1-channel CAN bus has 10 ID packets, and I only need the packets with two ids. How can I configure the forwarding for only these two ids?

0 件の賞賛
返信
1 返信

1,093件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi

Hope you are doing well

Refer the Document Number: AN13423 (Using CAN2CAN, CAN2ETH and ETH2CAN Features of LLCE on S32G ).  There are also example in s32ds as Can_Llce_Ds_Can2Can_S32G274a_M7 which show the internal routing functionality of CAN_LLCE Driver

 

Regards ,

Tushar

 

0 件の賞賛
返信