Question about S32G3 LLCE can2can and can2eth function kernel support version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about S32G3 LLCE can2can and can2eth function kernel support version

Jump to solution
1,023 Views
GG0712
Contributor III

Hi NXP team,

 

LLCE CAN controller start to support can2can, can2eth, ...  function from BSP38 kernel 5.15

I have lots of questions about this feature.

  1. Does S32G3 Linux kernel 5.10 support these feature?
  2. Does can2eth and eth2can support to custom ethernet switch or GMAC eth0 ?
    I can not found how to use in LinuxBSP User Manual
  3. Can I use this function without enabling m core?

 

Thanks

0 Kudos
Reply
1 Solution
1,003 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @GG0712 

Thanks for your post.

1. No, I checked the code and it is not enabled in BSP38-5.10 kernel.

2. No, only PFE is supported.

3. Yes, it is supported, you may reference the LLCE chapter of BSP UM for details.

 

BR

Chenyin

View solution in original post

0 Kudos
Reply
1 Reply
1,004 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @GG0712 

Thanks for your post.

1. No, I checked the code and it is not enabled in BSP38-5.10 kernel.

2. No, only PFE is supported.

3. Yes, it is supported, you may reference the LLCE chapter of BSP UM for details.

 

BR

Chenyin

0 Kudos
Reply