QSPI NOR memory support in Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QSPI NOR memory support in Linux

Jump to solution
3,546 Views
bou6
Contributor I

I am using S32g eval board and Linux bsp24, I want to to write and read from Qspi Nor memory, normally that should be supported by the mtd driver, but what I noticed is: first there is no qspi node in the dts file, second the mtd device files under /dev are not created.

My questions :

1- How is writing and reading in qspi Nor is handled ?

2- Can you please share basic examples for reading and writing in the QSPI Nor Memory ? 

0 Kudos
Reply
1 Solution
3,524 Views
bpe
NXP Employee
NXP Employee

You are using a BSP release which is very much obsolete. Consider moving to
the most recent BSP 29 HF1. Visit this link to enter the SDK download procedure. See BSP 29 HF1 User Manual Section 3.2.5.2 on how to write to
QSPI-based MTD partitions and boot from it.

Hope this helps,
Platon

View solution in original post

0 Kudos
Reply
2 Replies
3,513 Views
bou6
Contributor I

Thank you for for the answer, yes it is supprted in the BSP29, thank you 

0 Kudos
Reply
3,525 Views
bpe
NXP Employee
NXP Employee

You are using a BSP release which is very much obsolete. Consider moving to
the most recent BSP 29 HF1. Visit this link to enter the SDK download procedure. See BSP 29 HF1 User Manual Section 3.2.5.2 on how to write to
QSPI-based MTD partitions and boot from it.

Hope this helps,
Platon

0 Kudos
Reply