QBV on S32G-VNP-RDB3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QBV on S32G-VNP-RDB3

2,218 Views
piaochunri
Contributor II

请问如何在S32G-VNP-RDB3 上配置QBV功能,谢谢!

0 Kudos
Reply
5 Replies

2,198 Views
chenyin_h
NXP Employee
NXP Employee

@piaochunri , 您好

RDB3板卡上的GMAC支持QBV,但是目前的BSP文档中没有相关正式的章节进行说明,按照经验,您可以先参考以下内容

https://man7.org/linux/man-pages/man8/tc-taprio.8.html

然后尝试利用TC命令来配置相关TSN的特性

 

BR

Chenyin

0 Kudos
Reply

2,196 Views
piaochunri
Contributor II
我需要在SJA1110上实现QBV,需要配置GMAC链接SJA1110吗?我看目前SJA1110就是一个支持QBV的网关,如果配置PFE链接SJA1110能否实现QBV?谢谢
0 Kudos
Reply

2,188 Views
chenyin_h
NXP Employee
NXP Employee

@piaochunri ,您好

感谢回复

我之前的回复是基于您直接使用RDB3上的普通网络端口的情况下。

如果您是使用RDB3上的SJA1110的egress port连接的网口的话,因为sja1110本身支持QBV,也就是其egress 端口支持基于时间的流量调度。那么,您可能不需要额外使用Host端的工具(比如TC)来进行相应配置。

 

BR

Chenyin

0 Kudos
Reply

2,183 Views
piaochunri
Contributor II

那请问在sja1110上配置QBV的方法是什么,是否有教程?是通过S32DS吧。

0 Kudos
Reply

2,158 Views
chenyin_h
NXP Employee
NXP Employee

@piaochunri 您好

SJA1110的FW修改和功能的设置需要通过SJA1110的SDK,这个SDK可以在S32DS中进行配置,修改和编译,最后烧写到SJA1110内部的FLASH使用。

 

BR

Chenyin

0 Kudos
Reply