Peripheral circuits difference between S32G274A Mask1N92V&Mask0P77B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Peripheral circuits difference between S32G274A Mask1N92V&Mask0P77B

1,061 Views
chengpei
Contributor III

Hello,

I want to upload binaries to the flash through JTAG using Lauterbach in our new board(serialboot mode),

it said, "B::SYStem.Mode PREPARE" and failed.

chengpei_1-1703682213371.png

The only difference about this new board is the S32G274 device,

chengpei_2-1703682575457.pngPS32G274ABVUC 1N92V SBAF2002A(old one works fine), 

chengpei_3-1703682598264.pngS32G274AABVUC 0P77B SBCB2119A(new one failed).

So, do we have to do any modifications of the peripheral circuit when we replace 1N92V with 0P77B?

What modifications do I have to do?

Thank you very much! 

 

 

 

0 Replies