PMIC example build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC example build error

1,678 Views
77373
Contributor II

Hi NXP team,

When I import the Pmic_Configuration_Non_Autosar_Example_S32G399A_M7 project, a compilation error occurs. Could you help me resolve this issue? Thanks in advance!

RTD version: 5.0.0 D2410

77373_0-1762844312899.png

 

0 Kudos
Reply
3 Replies

1,657 Views
Joey_z
NXP Employee
NXP Employee

hi,77373

Thank you for contacting us.

Do you have finished the "Update Code" as the following picture?

Joey_z_0-1762845721582.png

 

BR

Joey

0 Kudos
Reply

1,652 Views
77373
Contributor II
Hi Joey_z,
Thank you for your response.
Yes, I did. This error occurred after "Update Code".
0 Kudos
Reply

1,638 Views
77373
Contributor II
Hi all,

Thanks a lot for your support, this issue has been fixed.
0 Kudos
Reply