NXP S32G3:Secure boot for bootloader:Issue in HSE_Init after reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP S32G3:Secure boot for bootloader:Issue in HSE_Init after reset

4,363 Views
kavyapk
Contributor I

Hello ,

I am using Board: S32G399RDB3 with an AUTOSAR application and NXP Boot on the M7 core.

HSE vesrion:HSE_DEMOAPP_S32G3XX_0_2_51_0

we are doing secure boot for bootloader with smr and cr configuration (preboot verification).

we are installing smr and publishing sysimage, we are performing mcu reset.  After this  hse init is not happening.  It is stuck in the loop given below

Capture.PNG

 

Could you please help us for understanding the HSE  behaviour 

0 Kudos
Reply
9 Replies

4,344 Views
kavyapk
Contributor I
Hi,
For the initial state before secure boot configuration and during secure boot configuration , the status bit for set for HSE_STATUS_INIT_OK and HSE_STATUS_RNG_INIT_OK . But after the smr install and sysy image publish when we perform reset ,there after these status bits are cleared.
Could you help us to understand this hse behaviour
0 Kudos
Reply

4,319 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @kavyapk, 

I'm working in your issue. I'll come ASAP with further information.

0 Kudos
Reply

4,264 Views
kavyapk
Contributor I

Hello,


I am putting some of our observations here


1.Initilally we thought Hse shutdown happened ,that is why init status we are not getting.But as per HSE_H reference manual ,if we do functional reset we should get the hse_status_init_ok, and we tried and still the bit was not set.


2.Second thing is from reference manual which says HSE_STAUS_INIT will set only after post boot verification is suuceessful.Capture1.PNG

So I would like to understand on this since we are getting HSE_STATUS_BOOT_OK after reset and but not the HSE_STATUS_INIT_OK.

In CR configuration we are proposing prebootsmr map,as shown below.Capture2.PNG

Is this is enough for secure boot smr verification or do we have to do both preboot and postboot smr map in CR entry .

We are asking beacuse in the above mentioned firmware manual snip there are saying about 3 stage verification.

Could you please comment on this scenario

 

0 Kudos
Reply

4,231 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @kavyapk,

Your issue seems to not be related to your SMR configuration. 

What I'm understanding is that when you perfom the mcu_reset as fuctional reset you get both bits cleared (HSE_STATUS_INIT_OK and HSE_STATUS_RNG_INIT_OK). 

At your code at HSE_FW_INSTALL_SEC_BOOT. Did you maintain the following?

HSE_MU_SendEvent(HSE_HOST_PERIPH_CONFIG_DONE);

Also, your SMR Entry config looks to be set properly.

In case you don't have the SendEvent fuction before the status check please add it and retry.

 

Let me know your results

 

0 Kudos
Reply

4,209 Views
kavyapk
Contributor I

Hello @carlos_o ,

Thankyou for your response

Yes I am already sending this event before checking status,

Capture.PNG

 

0 Kudos
Reply

4,176 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @kavyapk,

Thanks for clarifying.

Could you please run the Demo App without modifications to verify if your SoC are working properly? 

0 Kudos
Reply

4,142 Views
kavyapk
Contributor I

Hello @carlos_o ,

 

As per the log we are getting from console reagarding other HSE status other that RNG init and HSE init before and after the reset it shows soc is working properly.

Below shown is the console after secure boot config and followed reset

After reset console logAfter reset console log

0 Kudos
Reply

4,095 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @kavyapk,

Thanks for sharing you console output after reset.

I want to see if you get the HSE_STATUS_RNG_INIT_OK and HSE_STATUS_INIT_OK from the example or if you have the same behavior as you application. 

0 Kudos
Reply

4,050 Views
kavyapk
Contributor I
Hello @carlos_o,
We have checked with demo app also,there we are observing clock init issue .
0 Kudos
Reply