LLCE report LLCE_ERROR_MB_NOTAVAILABLE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLCE report LLCE_ERROR_MB_NOTAVAILABLE

1,362 Views
tommychen1986
Contributor II

Hi, we are developing  gateway with S32G274A.we found LLCE will report LLCE_ERROR_MB_NOTAVAILABLE sometimes. when it happened , it will not stop reporting error message until the can bus disconnect. 

Can you tell me why it hanppened?how can i resolve this problem?

Tags (1)
0 Kudos
Reply
3 Replies

1,356 Views
Joey_z
NXP Employee
NXP Employee

hi,tommychen1986

Do you use our RDB2 or customer board? which llce demo and version are you using in A/M core? are you using EB or S32DS IDE?

I am looking forward to your reply.

BR

Joey

0 Kudos
Reply

1,349 Views
tommychen1986
Contributor II

I'm using customer board. And the llce version is 1.0.5 in M core., AND IDE is EB.

0 Kudos
Reply

1,337 Views
Joey_z
NXP Employee
NXP Employee

hi,

The LLCE_ERROR_MB_NOTAVAILABLE is reported by the LLCE_RX module, that means the data is lost from Rx. It is suggested that increasing the HOH number of Rx filters can improve it.

BR

Joey

 

0 Kudos
Reply