LLCE FlexRay configuration on S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLCE FlexRay configuration on S32DS

882 Views
Yang_C
Contributor IV

Hi, 

I am encountering a configuration issue for LLCE FlexRay on S32DS.

I would like to set this parameter to TRUE, after spending a long time on the IDE, still could not find the right place to change it. Is there someone can provide any clue?

My IDE version is S32DS3.5.10.

Thank you in advance.

LLCE_FlexRay_Config.png

 

Tags (1)
0 Kudos
Reply
8 Replies

697 Views
Joey_z
NXP Employee
NXP Employee

Hi,Yang_C

Regarding "repeatTx", the driver is supported, but the interface configuration interface in EB is not. The main reason is that "repeatTx" is not a standard ECUC configuration item defined by the AUTOSAR FlexRay Interface (FrIf) specification, but rather an underlying Message Buffer extension attribute of the NXP FlexRay_IP Driver.

BR

Joey

0 Kudos
Reply

665 Views
Yang_C
Contributor IV

Thank you Joey. I will try manually update.

0 Kudos
Reply

674 Views
Yang_C
Contributor IV

Hi Joey,

Thanks for your reply, I am a little bit confused because you mentioned EB does not support configuring 'Repeat TX', but I am using S32DS. Wondering if S32DS support set repeat TX for FlexRay?

 

BR,

Yang

0 Kudos
Reply

670 Views
Joey_z
NXP Employee
NXP Employee

Hi,Yang_C

Thank you for your reply.

The S32DS is also not configurable and needs to be manually modified, but there are drivers that can achieve this function. 

BR

Joey

 

0 Kudos
Reply

845 Views
Joey_z
NXP Employee
NXP Employee

Hi,Yang_C

Thank you for contacting us.

What version of LLCE are you using? And are you using S32G2 or S32G3?

BR

Joey

0 Kudos
Reply

813 Views
Yang_C
Contributor IV

Hi Joey,

I am using S32G399 with S32DS3.5.10, LLCE 1.0.7, RTD 4.0.2. 

BR,

Yang

0 Kudos
Reply

784 Views
Joey_z
NXP Employee
NXP Employee

Hi,Yang_C

This seems to be an issue with the software itself. I will assist you in confirming it with the internal software developers!

BR

Joey

0 Kudos
Reply

781 Views
Yang_C
Contributor IV

Hi Joey,

 

Thank you for your help.

Looking forward to you reply.

BR,

Yang

Tags (1)
0 Kudos
Reply