LLCE CAN/CANFD General Driver(non Autosar) for M7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LLCE CAN/CANFD General Driver(non Autosar) for M7

1,111件の閲覧回数
yqlau
Contributor II

I'm working on the LLCE CAN/CANFD communication implement in a project for the M7 cores. I installed S32DS.3.4_LLCE_Addon_updatesite_1.0.4_signed.zip in the S32DS 3.4. I created a llce CAN project from the sdk, but I can only find the example for autosar. The llce driver is included in the MCAL.

Is there a general LLCE CAN/CANFD demo (non Autosar)for M7 core? Or how can I add the driver in the drivers component for a non Autosar application ?

0 件の賞賛
返信
1 返信

1,097件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

At this point in time, only the "LLCE Driver + Firmware" is available under the NXP site. As you are saying, the CAN driver is only available with AUTOSAR compliance.

Please, let us know if this information was helpful or not.

0 件の賞賛
返信