Keep trigger FCCU alram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Keep trigger FCCU alram

957 Views
Jeff-CF-Huang
Contributor III

Hi Sir,

I set all NCFs to S32CC_FCCU_REACTION_ALARM, and now the system continuously reports an FCCU alarm.

   89.474254] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   90.023262] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   90.570819] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   91.119105] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   91.667383] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   92.215727] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   92.763956] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   93.312249] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   93.860522] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   94.408812] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   94.957090] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   95.505383] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   96.053657] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   96.601946] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   97.150226] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   97.698512] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0
[   98.246801] s32cc_fccu 4030c000.fccu: Cleared faults 0x200000 from NCF_S2 (1) state=2->0


Best regards,
Jeff Huang

0 Kudos
Reply
1 Reply

924 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Jeff-CF-Huang 

Thanks for your post.

May I know if it is still found from BSP40 on S32G3 custom board? would you mind sharing the modification upon the default settings?

 

BR

Chenyin

0 Kudos
Reply