IPv6 Configuration @ RDB32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPv6 Configuration @ RDB32

2,659 Views
Atkinson
Contributor V

Hi, 

I am looking to use IPv6 address to Tx and Rx and completely replace with IPv4 address with IPv6 address in Transmission of Message 
How can i bring up IPv6 Address ?
what setup need to be done to implement in lwIP stack IPv6 after enabling it 
Looking forward for reference documents with respect to IPv6 in RDB Board
To replace the IPv4 with IPv6 how to do ? whether it is possible to replace?

Regards 
Atkison 

Tags (2)
0 Kudos
Reply
6 Replies

2,604 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Atkinson 

Thanks for your reply.

With the settings for enabling IPv6, then the stack would support both ipv4 and ipv6, if you do want to only use the ipv6, then undefine of the ipv4 would be required.

Besides, you may need to set a ipv6 address for the test, for example, 

 

0 Kudos
Reply

2,159 Views
Atkinson
Contributor V

Hi @chenyin_h 

The IPv6 needs to implemented from SJA1110 switch or S32G Processor which one it need to be done?
So how can we make a communication via IPv6 using LWIP how to derive a Standalone use case in implementing it.

Regards
Atkinson

0 Kudos
Reply

2,633 Views
chenyin_h
NXP Employee
NXP Employee

Hi, @Atkinson 

Thanks for your reply.

I am wondering the accurate version number of the S32G TCP/IP Stack, which version you are using from the following? 

chenyin_h_0-1752038492526.png

In general, by default, ipv6 is not supported, by setting the following to 1 would help to enable the ipv6

chenyin_h_1-1752039496593.png

 

BR

Chenyin

 

0 Kudos
Reply

2,629 Views
Atkinson
Contributor V

Hi @chenyin_h 

I am using the TCP/IP lwIP version - "SW32G_TCPIP_1_0_4_D2310_updatesite.zip"
I could see in code that i have option IPv6 enable and also i Have a option in TCP/IP middleware configuration ---> where i have ENABLE IPv6 option
I am looking to use IPv6 address to Tx and Rx and completely replace with IPv4 address with IPv6 address in Transmission of Message 
I am looking for a option to completely replace IPv4 with IPv6 address
Making a primary utilization of IPv6 in all aspects how to implement?

Regards
Atkinson 

Tags (1)
0 Kudos
Reply

2,638 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Atkinson 

Thanks for your post.

1. Seems you are working with M core application? are you using the S32G - TCP/IP Stack? if yes, which version? 

2. In general, the latest S32G - TCP/IP Stack released by NXP is based on Lwip2.1.x, as a result, the IPv6 could be supported, for the details guide for using/setting the stack, I suggest referencing the official document from https://www.nongnu.org/lwip/2_1_x/group__lwip__opts__ipv6.html

 

BR

Chenyin

0 Kudos
Reply

2,636 Views
Atkinson
Contributor V

Hello @chenyin_h 

Yes, I am working with M-Core Application
Yes using the TCP/IP Stack having a version of lwIP 2.1.2
I am looking to use IPv6 address to Tx and Rx and completely replace with IPv4 address with IPv6 address in Transmission of Message 
How can i bring up IPv6 Address ?
what setup need to be done to implement in lwIP stack IPv6 after enabling it

Regards
Atkinson

0 Kudos
Reply