IPCF is non-functional after the Linux kernel is locked down.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IPCF is non-functional after the Linux kernel is locked down.

1,461 次查看
Jeff-CF-Huang
Contributor III

Hi Sir,

IPCF is non-functional after the Linux kernel is locked down.

JeffCFHuang_0-1736144875557.png

Is there an alternative way to resolve it?

Best regards,

Jeff Huang

0 项奖励
回复
3 回复数

1,444 次查看
Joey_z
NXP Employee
NXP Employee

hi,Jeff-CF-Huang

In order to provide better support,can you provide more information?

Do you use custom boards?If not ,is it an RDB or EVB board?In addition ,which version of IPCF and BSP do you use?

According to your output information,There may be a conflict in the shared memory that IPCF tries to access.Do you follow the operation implemented by AN13750?

 

BR

Joey

0 项奖励
回复

1,431 次查看
Jeff-CF-Huang
Contributor III

Hi Joey,

The IPCF functions correctly when the lockdown feature is disabled.

The kernel enables LOCK_DOWN_KERNEL_FORCE_CONFIDENTIALITY to enhance security by blocking access to /dev/mem and /dev/kmem, which could otherwise allow reading or writing to kernel memory.

This issue persists consistently, regardless of the IPCF or BSP version.

Best regards,
Jeff Huang

0 项奖励
回复

1,386 次查看
Joey_z
NXP Employee
NXP Employee

Hi,Jeff-CF-Huang

Sorry for the late reply.

You should check if there is a conflict between the memory specified when the lockdown feature is enabled and the  memory set by IPCF. If there is a conflict, you need to change it to a different address.

BR

Joey

0 项奖励
回复