How to switch from M-core to A-core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to switch from M-core to A-core

2,414件の閲覧回数
Atkinson
Contributor V

Hello,
I would like to switch from M-core to A-core how to do that in S32G VNP-RDB32 Board
Currently i would see the S32G VNP-RDB Board is using the M single core 
How to bring A-53 Core in S32G VNP RDB Board, how to do 

whenever i am using the S32G VNP RDB Board its using the Single core for processing the things in documentation totally we have 8 - cores how to bring the S32G to use the Different 8 -cores in the implementation how to bring that 

Regards
Atkinson 

タグ(1)
0 件の賞賛
返信
7 返答(返信)

2,241件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Atkinson 

Thanks for your reply.

I feel sorry that there is not a directly link for downloading the BSP43.0 UM, it could be found in the BSP images downloading page from your account.

For issues that need to be shared with some private information, we suggest raising new support ticket via support.nxp.com.

Thanks for your understanding.

BR

Chenyin 

0 件の賞賛
返信

2,289件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Atkinson 

Thanks for your reply.

1. The best guide for directly booting the board via A53 is the BSP UM, for now, I suggest reading BSP43.0 UM for details; for using M7 bootloader and the A53 BSP together, the AN13750 would be the correct choice.

2. I feel sorry that there are not such documents formally provisioned by NXP, I apologize.

 

BR

Chenyin

 

BR

Chenyin

0 件の賞賛
返信

2,280件の閲覧回数
Atkinson
Contributor V

Hello @chenyin_h 

can you share me the link of document BSP43.0 UM 

BR
Atkinson

0 件の賞賛
返信

2,342件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Atkinson 

You are welcome

1. In general, the A53 cores could be brought up via A53 bootloader(BootROM->TFA) directly, or by the M7 bootloader(BootROM->M7 Bootloader->TFA).

2. It is possible to either running FreeRTOS or AUTOSAROS on RDB2,  it is also possible to run the FreeRTOS on one M7 core, while running AUTOSAROS on the other M7 core.

 

BR

Chenyin

0 件の賞賛
返信

2,306件の閲覧回数
Atkinson
Contributor V

Hello @chenyin_h 

I would like to know more about the accessing the cores 
1.) How to do that, is there any documentation specify how to access the A53 Cores Bootloader or via through M7 Bootloader accessing the A53 
2.)How to do that, for this also any documentation is there to do running AUTOSAROS on the M7 core or A53 core or the each core utilization which uses different Core in RDB32 Board

タグ(1)
0 件の賞賛
返信

2,388件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Atkinson 

Thanks for the post.

Generally, S32G274 is on the RDB2, there are 3 M7 cores and 4 A53 cores within the SOC.

From NXP's perspective, BSP is provided for bring up the board via A53 cores, while M core SDK(RTD) is provided as the base for bringing the board via M7 cores, so there are software provided for both M7 and A53 cores.

For M7 side, usually different applications are running on different cores, and for A53 side, usually the 4 cores are managed in one OS(Linux SMP).

For using all cores on RDB2, there is a recommended method, which is in detailed shown in AN13750, I suggest reading it for further reference.(https://www.nxp.com/webapp/Download?colCode=AN13750)

 

BR

Chenyin 

 

0 件の賞賛
返信

2,374件の閲覧回数
Atkinson
Contributor V

Hello @chenyin_h 
Thanks for the Reply!

So "for A53 side, usually the 4 cores are managed in one OS(Linux SMP)" how to bring this up ?
Whether in S32G274A is it possible to switch it from FreeRTOS Compliant to AUTOSAR Compliant?

Regards 
Atkinson

タグ(1)
0 件の賞賛
返信