How to integrate the EB Tresos generated code into S32DS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to integrate the EB Tresos generated code into S32DS?

1,074 Views
viswa_kondapall
Contributor IV

Hi,

We are working on CAN2CAN project based on GOLDVIP-RDB2 board. We configured CAN0/1/2 in EB tresos, generated the code for the same. 

Now how to create a project in S32 Design studio for the generated folder. attached below the generated.zip file.

Regards,

Viswa

0 Kudos
Reply
1 Reply

1,057 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

There are some available guides regarding creating a project using S32DS. Below will be a link redirecting to these HOWTO's.

S32DS - list of HOWTOs - NXP Community

As to integrating other files to your project, you have to create the correct links in order for your project to be able to see them. This can be made manually from the project properties.

Also, S32DS integrates Config Tools, which also allows for creating configurations similar to EB Tresos, which could make the development easier.

Please, let us know if this information was helpful or not.

0 Kudos
Reply