How to encypt with AES algo on #S32G3 - RDB3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to encypt with AES algo on #S32G3 - RDB3

1,632 次查看
Liuliyuan
Contributor II

Hello,

We are trying to test AES encrypt and decrypt function with the HW of HSE on RDB3 board. We tried PKCS11-tool and Opnessl , none  worked. Could you please help have a check?

  1. PKCS11-tool

 ~/pkcs11-tool\                                                                                           

>  --module /usr/lib/libpkcs-hse.so.1\                                                                                             

>  --encrypt\                                                                                                                      

>  --mechanism AES-CBC\                                                                                                            

>  --id 000101 \                                                                                                                   

>  --iv 0123456789abcdef0123456789abcdef\                                                                                          

>  --input-file file1.txt\                                                                                                         

>  --output-file file1_pkcs11.dat                                                                                                  

libhse: initialized, firmware status 0x6b20                                                                                        

Using slot 0 with a present token (0x0)                                                                                            

Using encrypt algorithm AES-CBC                                                                                                    

libhse: service response 0xA5AA5317 on channel 5                                                                                   

libhse: read reply failed on channel 5                                                                                             

libhse: closed                                                                                                                     

error: PKCS11 function C_EncryptUpdate failed: rv = CKR_FUNCTION_FAILED (0x6)                                                      

Aborting.                                                                   

2. OPENSSL

2.1 With -K parameter, key is provided directly.  One failure reported and one blank file created. The log as below:

 openssl enc -engine pkcs11 -aes-128-cbc -in file1.txt -out file1_HWenc.dat -iv 0123456789ABCDEF0123456789ABCDEF  -K 0123456789ABCDEF0123456789ABCDEF -debug                                                                                  

Engine "pkcs11" set.                                                                                                               

ctx_load_object returned NULL                                                                                                      

BIO[0x55ad1bd370]: ctrl(6) - cipher                                                                                                

BIO[0x55ad1bd2a0]: ctrl(6) - FILE pointer                                                                                          

BIO[0x55ad1bd2a0]: ctrl return 0                                                                                                   

BIO[0x55ad1bd370]: ctrl return 0                                                                                                   

BIO[0x55ad1bd030]: ctrl(10) - FILE pointer                                                                                         

BIO[0x55ad1bd030]: ctrl return 0                                                                                                   

BIO[0x55ad1bd030]: ctrl(2) - FILE pointer                                                                                          

BIO[0x55ad1bd030]: ctrl return 0                                                                                                   

BIO[0x55ad1bd030]: read(0,8192) - FILE pointer                                                                                     

BIO[0x55ad1bd030]: read return 1 processed: 367                                                                                    

BIO[0x55ad1bd370]: write(0,367) - cipher                                                                                           

BIO[0x55ad1bd370]: write return 0 processed: 0                                                                                     

error writing output file                                                                                                          

BIO[0x55ad1bd030]: Free - FILE pointer                                                                                             

BIO[0x55ad1bd2a0]: Free - FILE pointer                                                                                             

BIO[0x55ad1bd370]: Free - cipher           

 

2.2 When we try to load key from HW, we cannot find a right parameter to use. -inkey/-key/-keyform are not supported on "openssl enc"

 

Many thanks.

0 项奖励
回复
3 回复数

1,612 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We assume that you are trying to implement this under Linux, is this correct?

If so, can you let us know which BSP version are you using?

Please, let us know.

 

0 项奖励
回复

1,603 次查看
Liuliyuan
Contributor II
Hi,
Yes,we are working on Linux. The BSP version is 40.0.
Thanks
0 项奖励
回复

1,582 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. 

All information on regards of HSE/Crypto usage under BSP40 are provided under the BSP40 User Manual for S32G3 platform.

Aside from that, we are not seeing much information on regards of PCKS11 and openssl usage, since we understand is not supported directly by NXP. For that, we can recommend contacting the related support team.

We do apologize.

Please, let us know.

0 项奖励
回复