How do I enable UART2 in S32G2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I enable UART2 in S32G2

2,116 Views
jack_huang1
Contributor IV

Dear,

         Now we are using NXP S32G274 platform. BSP is based on BSP34 version. How to enable UART2 in BSP34? At present, some configuration information is added to kernel DTS (as follows), but it has no effect (unable to read and write data), specifically as follows:

         

 &pinctrl {

            .......

            uart2_pins: uart2 {

                  uart2_grp0 {

                          pinmux = <S32CC_PINMUX(64, FUNC2)>;

                          output-enable;

                          slew-rate = <S32CC_SLEW_83MHZ>;

                  };

                  uart2_grp1 {

                           pinmux = <S32CC_PINMUX(737, FUNC0)>;

                           input-enable;

                           slew-rate = <S32CC_SLEW_83MHZ>;

                  };

                  .......

            };

   };

 

    &uart2 {

              pinctrl-0 = <&uart2_pins>;

              pinctrl-names = "default";

              status = "okay";

    };

 

 Please check it,thank you!

 

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,055 Views
nxf92355
NXP Employee
NXP Employee

Hi Jack 

I am not finding BSP34 . Please use latest BSP35

Thanks 

Tushar 

0 Kudos
Reply

2,066 Views
nxf92355
NXP Employee
NXP Employee

Hi Jack 

Are you using custom bard or EVK board likeRDB2 ?

Thanks 

Tushar 

0 Kudos
Reply

2,083 Views
mz_001
Contributor I

大哥,搞定了没

0 Kudos
Reply