Goldbox VIP source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Goldbox VIP source code

2,824 Views
Vishnu13
Contributor I

We want to build applications on NXP goldbox, but currently only the pre-built image is available to us. Is there a source code available for goldbox vip?? Or is there any alternative method? 

Labels (1)
0 Kudos
Reply
3 Replies

2,819 Views
gmocanu
NXP Employee
NXP Employee

Hello,

 

Parts of the GoldVIP source code are publicly available on CodeAurora Forum [1]. Also, besides the pre-built binaries, the GoldVIP deliverable includes other configuration files/source code that can be used to configure some of the GoldVIP applications. Could you be more specific about what parts of the GoldVIP you want to customize?

 

Best regards,

George


[1] - https://source.codeaurora.org/external/autobsps32/goldvip

0 Kudos
Reply

2,778 Views
Vishnu13
Contributor I

Hi,

What are the sample applications available with the pre-built image for Goldvip 1.3? Also is there any hardware requirement for those applications?

Thanks,

Vishnu

0 Kudos
Reply

2,765 Views
gmocanu
NXP Employee
NXP Employee

Hello,

 

All the applications and use cases available in GoldVIP are presented in the GoldVIP User Manual, which can be downloaded separately from nxp.com, or you can find it already included in the documentation directory from the GoldVIP deliverable (if we are talking about GoldVIP 1.3.0). Also, any hardware prerequisites are detailed in the aforementioned document.

 

Best regards,

George

0 Kudos
Reply