Flexray get stuck in FLEXRAY_STATE_STARTUP on two S32G-VNP-RDB3 boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexray get stuck in FLEXRAY_STATE_STARTUP on two S32G-VNP-RDB3 boards

890件の閲覧回数
HsinYu
Contributor I

Please support us to connect 2 Flexray node between 2 different S32G-VNP-RDB3 boards.

We’re working on following example code within S32 Design Studio V3.5 with S32 Debug Probe.

Flexray_ExternalCommuation_node1_S32G399A_M7

Flexray_ExternalCommuation_node2_S32G399A_M7

 

We also set GPIOs per schematic of S32G-VNP-RDB3 board as the attached below.

Screenshot from 2024-03-25 16-02-18.png

Nevertheless, pocState will get stuck in FLEXRAY_STATE_STARTUP and no more further transmit and receive from flexray bus.

Please help!

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)