Flash Tool Response error #3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Tool Response error #3

4,965 Views
234
Contributor I

   

   We use flashtool , when downloading the program to norflsh through s32G2 serial port 0, the serial port chip has been chaged, but 3 of the 5 boards appear to obtain the chip ID or display The Resolution error #3 is displayed when the algorithm is loaded.

   

error#3.PNG

 

The dialing code has been set to the all off state. After downloading the program through the burner, observe that the uart0 print message and receive information are normal.

What does the error #3 stand for? Are there special restrictions on the hardware of UART0, thank you.

 

 

我们使用Flash tool 软件,通过s32G的串口0下载程序到norflsh时,串口芯片已经更换,5块板子有三块出现在获取芯片ID或者加载算法时会显示Response error #3。

拨码已经调到all off 状态。通过烧录器下载程序后观察uart0打印信息和接收信息正常。

请问下载的error #3 代表什么?对于uart0 的硬件有无特别的限制,谢谢。

Tags (1)
0 Kudos
Reply
6 Replies

4,770 Views
sapna_12
Contributor II
Hey
Were you able to figure out why the #3 error was coming?
0 Kudos
Reply

4,932 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello 234,

You could have a try using the FlashTool command to write the image into QFlash, please refer to S32_Flash_Tool_User_Guide.

Regards

0 Kudos
Reply

4,894 Views
234
Contributor I

     We have try use  the FlashTool command to write the image into QFlash the response error also happen at Win10 system ,but we find when we use linux flashtool at  VMware ubuntu16 it works well.

So it's may be something wrong with windows flahtool,What's the default uart BdRate,we can't fond place to set it,Also we use a new ft4232 usb2uart chip.We just want use it in windows computer,

0 Kudos
Reply

4,916 Views
234
Contributor I

But we still can't download image,The error ais like this picture.

 But we still can't download image,The error alwaya like this.ResponseError.
捕获.PNG

 

0 Kudos
Reply

4,865 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

That error mean that the board is not responding, it is on; connected Could be many reason for that, but is not software issue.

 

Regards

0 Kudos
Reply

4,769 Views
sapna_12
Contributor II
Can you share what other reasons can be for the #3 error in Flash tool
0 Kudos
Reply