Fetcher error while building the image after including pfe pfe-slave in local.conf.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fetcher error while building the image after including pfe pfe-slave in local.conf.

358 Views
hulk101
Contributor III

I want to build PFE multi-instance driver, For which I have added "DISTRO_FEATURES:append = " pfe"" in the local.conf, and while bitbake I get the below error:

WARNING: pfe-1.0.0-r0 do_fetch: Failed to fetch URL file://./s32g_pfe_class.fw, attempting MIRRORS if available
ERROR: pfe-1.0.0-r0 do_fetch: Fetcher failure: Unable to find file file://./s32g_pfe_class.fw anywhere. The paths that were searched were:
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe-1.0.0/fsl-auto
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe/fsl-auto
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/files/fsl-auto
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe-1.0.0/s32g274ardb2
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe/s32g274ardb2
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/files/s32g274ardb2
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe-1.0.0/s32cc
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe/s32cc
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/files/s32cc
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe-1.0.0/s32
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe/s32
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/files/s32
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe-1.0.0/armv8a
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe/armv8a
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/files/armv8a
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe-1.0.0/aarch64
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe/aarch64
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/files/aarch64
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe-1.0.0/s32g
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe/s32g
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/files/s32g
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe-1.0.0/s32g2
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe/s32g2
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/files/s32g2
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe-1.0.0/aarch64
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe/aarch64
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/files/aarch64
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe-1.0.0/
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe/
/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/files/
/home/teuser/S32G2/fsl-auto-yocto-bsp/downloads
ERROR: pfe-1.0.0-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'file://./s32g_pfe_class.fw')
ERROR: Logfile of failure stored in: /home/teuser/S32G2/fsl-auto-yocto-bsp/build_s32g274ardb2/tmp/work/s32g274ardb2-fsl-linux/pfe/1.0.0-r0/temp/log.do_fetch.122939
ERROR: Task (/home/teuser/S32G2/fsl-auto-yocto-bsp/sources/meta-alb/recipes-kernel/pfe/pfe_1.0.0.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2128 tasks of which 2125 didn't need to be rerun and 1 failed.

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

308 Views
chenyin_h
NXP Employee
NXP Employee

Thanks for the reply, @hulk101 

From the log, the PFE FW is not found by the Yocto, have you added it according to the UM?

chenyin_h_0-1758180124137.png

 

BR

Chenyin

0 Kudos
Reply

306 Views
hulk101
Contributor III
Hi, @chenyin_h

NXP_FIRMWARE_LOCAL_DIR is not added. I have searched for the "s32g_pfe_class.fw" file and was not able to find it. Should I create this file by my own ?
0 Kudos
Reply

304 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @hulk101 

Thanks for your reply.

No, the file mentioned is the PFE FW which is provisioned by NXP, you may download it in your account, like this:

chenyin_h_0-1758188868304.png

Note that this is not the version used for BSP38, you may try downloading the 1.7.1 PFE FW for using with the BSP38.

I hope it will help.

 

BR

Chenyin

0 Kudos
Reply

326 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @hulk101 

Thanks for the post.

May I know which version BSP is used?

 

BR

Chenyin

0 Kudos
Reply

320 Views
hulk101
Contributor III
Hello @chenyin_h

BSP 38.0 version is used for the build.

Thankyou.
0 Kudos
Reply