Hi NXP,
Here is a problem about "faided to find an OP-TEE supplicant device" when I try to run optee exmaples in S32G BSP36 system.
I have edit /conf/local.conf and appended the following line:
DISTRO_FEATURES:append = " optee"
Then use "bitbake fsl-image-auto" to build the image.
When I try to run "tee-supplicant &", it report the error:
"ERR [263] TSUP:main:819: failed to find an OP-TEE supplicant device"
By the way, I find a warning print in booting BL31 as below:
NOTICE: BL2: Booting BL31
I/TC:
I/TC: Non-secure external DT found
I/TC: OP-TEE version: bsp36.0-3.18-dev (gcc version 11.3.0 (GCC)) #1 Fri Mar 24 13:56:10 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: Primary CPU switching to normal world boot
Could you help check it, and give some support to solve the problem?
Thanks.
已解决! 转到解答。
Hi @milon,
Thank you for reaching out to us.
It seems that during booting the Linux, the tee-supplicant is already loaded. you can check it by doing "ps -elf".
you can kill the already loaded tee-supplicant and run again or move forward with running the example application.
Hope this helps you.
Thanks,
Mayank s Patel
Hi @milon,
Thank you for reaching out to us.
It seems that during booting the Linux, the tee-supplicant is already loaded. you can check it by doing "ps -elf".
you can kill the already loaded tee-supplicant and run again or move forward with running the example application.
Hope this helps you.
Thanks,
Mayank s Patel