Ethernet Packets Loss

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet Packets Loss

846 次查看
KJNK
Contributor II

Hi, I am Naresh Kumar.
I am using the S32G274ARDB2 board. I am working on the ethernet part of this board. I am facing packet loss on the board
The board has pfe0,pfe1,pfe2 and eth0.
Port Mapping:
eth0 -> GMAC, pfe0 -> PFE_EMAC_0 , pfe1 ->PFE_EMAC_1, pfe2 ->PFE_EMAC_2

Issue:  When I simultaneously send the packets to 4 ports, I face packet loss in all ports. The PFE is configured as a Default
Interface     tx           rx
eth0        10lakhs  999111
pfe0        10lakhs  999980
pfe1        10lakhs  999698
pfe2        10lakhs  980964


Packets info:
No of packets: 10 lakhs  [4ports * 10lakhs =40lakhs]
Packet length = 1 packet has 1324 length , Data = 1284 bytes in one packet, Protocol = UDP
Speed :936 Mbps [Each port(Rx) is configured as 1Gbps,TX speed of 936 Mbps]
Time [Tx] = 15 sec

Please help me how to solve this issue.
Thank you
 

 

0 项奖励
回复
0 回复数