EtherNet/IP (CIP) Protocol Support on S32G3xx Platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EtherNet/IP (CIP) Protocol Support on S32G3xx Platform

788件の閲覧回数
P_lavanya18
Contributor I

Hello NXP Team,

I am currently evaluating the S32G3xx series for an industrial networking application and would like to confirm whether the platform supports the EtherNet/IP (CIP) protocol either natively or through available software stacks.

Specifically, I am interested in understanding:

  • Whether NXP provides any middleware or SDK support for EtherNet/IP (CIP)
  • If third-party stacks (e.g., OpENer or commercial CIP stacks) are compatible with the S32G3xx architecture
  • Any reference designs, application notes, or example projects related to EtherNet/IP on this platform

Your guidance on this would be greatly appreciated.

Best regards,
lavanya pandhila

タグ(1)
0 件の賞賛
返信
1 返信

765件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @P_lavanya18 

Thanks for your post.

As far as I know, the CIP(ethernet/IP) stack is not included by default within BSP/RTD, or public demo/document from NXP.

However, since the CIP stack is an application protocol, which is based on the TCP/IP. The opensource implementation like OpENer, they would be possibly used based on the BSP provisioned by NXP theoretically, I suggest integrating it yourself for a trial, for example,  using the ubuntu-based RFS during the integration work, in order for solving lib dependency more conveniently.

I hope it will help.

 

BR

Chenyin

0 件の賞賛
返信