Error from DDR tool in project based on S32G3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error from DDR tool in project based on S32G3

2,322 Views
Gonchar
Contributor II

I'm trying to use DDR tool to bring up DDR4 MT53D512M32D2DS on our board with S32G3 MCU. I set chip in serial boot mode and try to run "Firmware Init test", but tool finishs the process with Fail. I attached log to the post.

What is the reason for such kind of error?

Thank you!

0 Kudos
Reply
1 Reply

2,250 Views
MayanksPatel
NXP Employee
NXP Employee

Hi @Gonchar,

Hope you are doing good.

The issue seems in the serial module as the script accepts data serially and converts it into base 10.

Can you please check that "0xmw340000" was sent properly over serial communication? Are any changes are done on the board side?

 

Thanks,

Mayank s Patel

 

 

 

0 Kudos
Reply