Driver runtime error: [pfeng 46000000.pfe: ERR:(PFENG_DEV) event 19

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driver runtime error: [pfeng 46000000.pfe: ERR:(PFENG_DEV) event 19

1,651 Views
jackchen1
Contributor I

Dears,

          I used s32g274, BSP version: BSP32, PFE driver version:1.5.0, when add PFE driver, there is an error : " Driver runtime error: [pfeng 46000000.pfe: ERR:(PFENG_DEV) event 19 -TLITE Watchdog trigered:[pfe_wdt_csr.c126] " . what can cause this error?  thks~

0 Kudos
Reply
3 Replies

1,583 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @jackchen1 

Thanks for your reply.

Seems the PFE driver 1.5 only used on BSP38, along with the PFE firmware 1.7.1.

May I know if the customer still use the old PFE firmware in BSP32? which version firmware they were using?

 

BR

Chenyin

0 Kudos
Reply

1,625 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @jackchen1 

Thanks for your post.

1. May I know how to trigger this issue? on a RDB2 or custom board?

2. Since the BSP32 is relatively old, have your ever tried it with newer BSPs?

3. Furthermore, from BSP32 release notes, the PFE firmware 1.2.0 and PFE linux driver 0.9.7 are compatible version, from my opinion, the PFE linux driver 1.5.0 may not compatible with BSP32. then there may be possibly some unpredictable issues.

 

BR

Chenyin

0 Kudos
Reply

1,586 Views
jackchen1
Contributor I
Thks for your respond,
1、Custom board.
2、Custom didn't try newer BSP,because design for long time,They don't dare to upgrade the BSP.
3、Feedback from customer , they update PFE linux driver 1.5.0 because there was a memory leak occurred before. could you give some suggestions.
Thks~

cou
0 Kudos
Reply