Certificate slots

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Certificate slots

941 次查看
Jayateerth
Contributor I

Hi team,

Following are the Hardware details that I'm currently using,

Board: S32G399RDB3 with Autosar application in M7 core and BSP.V.40 used in the A core.

I am using the HSE Standard version, below are some of the questions I have,

1. I noticed that there are no certificate slots defined as "HSE_KEY_TYPE_ECC_PUB_EXT" in HSE. Is it required for me to use the HSE Premium version? If yes, then how do we get it?

2. Can we modify the HSE application code for the premium version SW package according to our requirements?

Thank you.

Regards,
Jayateerth

0 项奖励
回复
1 回复

917 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @Jayateerth 

Thanks for your post.

May I know which version HSE FW you are working with? I have checked the FW0.2.22, and found that HSE_KEY_TYPE_ECC_PUB_EXT is defined under hse_keymgmt_common_types.h, would you please double check on it.

For premium package related questions, I suggest submiting a ticket via the support channel, or contacting

your DFAE/FAE for further support on this topic.

 

BR

Chenyin

0 项奖励
回复